M-Series – Updating exacqVision Software

In order to comply with the NDAA  “National Defense Authorization Act”, a two-step process is required to update an M-Series. First you must upgrade to version 20.03, then the server and webserver can be upgrade to the latest version. exacqVision Client versions higher than 20.03 are not supported. Note: The exacqVision Client version should not be… Continue reading M-Series – Updating exacqVision Software

Updating Supermicro C7Q67 Motherboard Firmware

A small percentage of exacqVision systems with Supermicro C7Q67 motherboards installed have been found to exhibit widely fluctuating network performance and then lock up. The problem is known to occur only on systems containing Supermicro C7Q67 motherboards with theĀ BIOS firmware versionĀ 1.0b. These motherboards are found mostly in 2U exacqVision A Series and Z series servers.… Continue reading Updating Supermicro C7Q67 Motherboard Firmware