Deprecation of Legacy Installers – exacqVision 24.03 Update

As part of the exacqVision 24.03 software release, we are announcing the deprecation of specific installers that were previously part of the collection of software downloads available on the Exacq web site, https://exacq.com. What installers are being retired? On both Windows and Ubuntu – the 32-bit installers, also known as “x86” installers, of server, client,… Continue reading Deprecation of Legacy Installers – exacqVision 24.03 Update

Server 23.09 Fails to Run on Ubuntu 14.04 x86

Description Users with Ubuntu 14.04 x86 (32-bit) experience an error when attempting to install or update to ExacqVision Server version 23.09. <br> Product ExacqVision Server 23.09 x86 and above <br> Steps to Reproduce Attempt an update or fresh install of ExacqVision Server version 23.09 on a Ubuntu 14.04 x86 system. <br> Expected Results Installation without… Continue reading Server 23.09 Fails to Run on Ubuntu 14.04 x86

Can my NVR be Updated to Windows 10

Title Can my NVR be Updated to Windows 10   Description  For customers that would like to migrate from their current operating system to Windows 10, we offer a purchasable upgrade kit.  However you should first determine if the system is compatible / eligible for the upgrade.   Product  exacqVision ServerUbuntu Windows 7 Windows Embedded 7 (WES7) Solution… Continue reading Can my NVR be Updated to Windows 10

Updating Windows Operating System

Windows To update your Windows 10 Operating System: Open Windows Update by right clicking the Start button in the lower-left corner and select search. In the search box, type Update, and then, in the list of results, click either Windows Update or Check for updatesClick the Check for updates button and then wait while Windows looks for the latest updates for your computerIf you… Continue reading Updating Windows Operating System

Update Ubuntu Linux Software Using Command Line

Installing updates via Terminal The commands are as follows: apt update: Update is used to resynchronize the package index files from their sources on Ubuntu Linux via the Internet.apt upgrade: Upgrade is used to install the newest versions of all packages currently installed on the Ubuntu system. To update software list for Ubuntu First, open… Continue reading Update Ubuntu Linux Software Using Command Line

ExacqVision stance on Operating System updates

The official stance of ExacqVision regarding security updates and auto-updates is they are off by default, because there is the potential risk of the NVR being rebooted during the update process which can stop video recording, so please plan accordingly!!! ExacqVision cannot control the integrity of security patches or operating systems updates; therefore these off… Continue reading ExacqVision stance on Operating System updates

How to Update 2TB WD Firmware

Steps Download the OS-appropriate WD_x compressed file (Windows or Linux) to the desktop.WD_LinuxWD_WindowsUncompress the fileWindows:Right click WD_Windows.zip and choose “Extract All…”Linux:Open Terminal and type sudo tar -xvf WD_Linux.tar.gzStop the exacqVision Server service.Open a Command Prompt or Terminal and navigate to the WD_x folder.The process varies here, depending on the OS. In the Command Prompt or Terminal, type:Windows:WD_download.exe RR04.pkgLinux:sudo chmod 775… Continue reading How to Update 2TB WD Firmware

Update web service for Apache httpoxy vulnerabilities

Description The version of Apache embedded in the web service has been found to expose a security vulnerability, known as “httpoxy” (technical details: ​CVE-2016-5387). This vulnerability can be avoided by changing the configuration of Apache. <br> Version Introduced 2.3.9 <br> Platform Web Service / All <br> Work Around Open the evApache httpd.conffile for editingWindows: C:\Program Files\exacqVision\WebService\evApache\conf\httpd.confLinux: /etc/evapache/httpd.confFind and change… Continue reading Update web service for Apache httpoxy vulnerabilities

Unable to Edit Web Service Scheduled Update in ESM

Symptom: When scheduling an update to a web service through ESM, a user cannot edit the scheduled update.  <br> Problem: Clicking on the Edit option for a scheduled update to a web service from within ESM results in an error.  This can be seen from the Web Services page when clicking to the Web Service… Continue reading Unable to Edit Web Service Scheduled Update in ESM

How to update the M-Series recorder

** IMPORTANT ** Before updating please review Knowledge Base Article #6655 “M-Series – Updating exacqVision Software” for important information. M-Series recorders currently can be updated using two methods. ** IMPORTANT ** Before updating please review Knowledge Base Article #6655 “M-Series – Updating exacqVision Software” for important information. <br> Related Articles <br>