ESM returns error when converting 31+ character Unmanaged server user to Managed

Affected platforms ESM 3.0 or later <br> Symptom An attempt to convert an unmanaged server user to a managed server user that contains more than 30 characters in the username will return a red banner displaying the following error: “Value too long for type character varying(30).” Also note that any usernames greater than 36 characters… Continue reading ESM returns error when converting 31+ character Unmanaged server user to Managed