Description -When updating Windows 10 and rebooting the Exacq unit, it will not come back to boot up again and has to power off manually and power on the unit again on Motherboard “ASRock H110E1” with Firmware version 1.50 Solution The Motherboard BIOS Firmware needs to be updated to version 1.60A The instructions to update… Continue reading Exacq Server is not booting after the windows update reboot.