Description Customer was getting odd results when trying to edit the name of either a group or username in EM. Product exacqVision Enterprise Manager 21.06exacqVision Enterprise Manager 22.09 Steps to Reproduce From the EM dashboard access either Users or GroupsSelect an existing user or group Click the pencil icon to edit Change the name of… Continue reading Unexpected Results When Updating Groups or Users in exacqVision Enterprise Manager
Tag: Unexpected Errors
How to Disable/Enable exacqVision Watchdog Timer
Description Built by Exacq “BBE” NVRs utilize a watchdog timer, which during normal operation is reset every second. If the watchdog timer has not been reset within 60 seconds it will trigger a system reboot. The assumption being that machine is in a bad state. For various troubleshooting reasons you may need to disable/enable the… Continue reading How to Disable/Enable exacqVision Watchdog Timer