Unable to Start Web Service on Windows 10

Problem Users installing the exacqVision web service on Windows 10 machines find that the exacqVision web service is not enabled and encounter errors when attempting to manually start the service. <br> Cause This is due to a port conflict. The default port used by evApache is port 80. This is also the default port for… Continue reading Unable to Start Web Service on Windows 10