iSCSI CONSIDERATIONS WITH LINUX RECORDERSAlso Note: https://crm.exacq.com/kb/?crc=42338 == recovering corrupt iSCSI configuration in Linux (open-iscsi issue). This can also solve the occasionally-observed problem of deleting a portal, restarting service, and observing the portal was not actually deleted after all. Alternatively, you can also: sudo services edvrserver stopsudo apt-get purge open-iscsisudo apt-get install open-iscsisudo services edvrserver start… Continue reading iSCSI CONSIDERATIONS WITH LINUX RECORDERS
Tag: Una Systems
Illustra discovery for Pro and Essentials issues with dual nic as well as Una systems
Inconsistent results. Web interface not showing all details, firmware, model, etc. Doesn’t always find Pro cameras even though static IP addressed. Also found 610LT’s twice and added them twice.Workaround suggestedFor Dual nic systems:For dual nic systems with duplicated results, either disable one of the nic’s or make sure that they are not set to the… Continue reading Illustra discovery for Pro and Essentials issues with dual nic as well as Una systems