Affected platforms Una LC-Series server with exacqVision Server 7.2 <br> Symptom When an EasyConnect camera is plugged into an Una POE port, the camera is automatically discovered, but never automatically addressed. This is due to the camera being discovered with an empty MAC address. <br> Workaround This issue is intermittent, so clicking to rescan or… Continue reading Una discovers EasyConnect camera but doesn’t automatically address and connect
Tag: Una LC-Series
System watchdog after changing time on an Una
Una systems may watchdog after changing the system clock backwards. To disable usbdio watchdogs, add this to usbdio.ini: watchdog=0 If Una is the 16 port version, the above line will need to be added to both device sections in usbdio.ini.