Description Meaning of the UBAD or UGOOD messages, most commonly seen in RAID Controller, but may appear in Storage. Product Information Solution If the same disk, moved to another slot, goes back to the UBAD status, the disk itself is bad. Replace the drive.If the previously good drive, moved into the same slot, goes into… Continue reading exacqVision UBAD / UGOOD Messages
Tag: UGOOD
2021-02 – Hard Drive Issues Training
Hard Drive Issues Troubleshooting