Description Server crashes when deleting a UDP serial port. The crash happens for both the stand-alone UDP serial port or the Neo internal serial port. <br> Introduced 8.4 <br> Workaround Workaround is to disable the UDP serial port before deleting it. To disable a stand-alone UDP serial port, set the usage type to None. To… Continue reading Crash when deleting UDP serial port