Using the Axis I8116-E Network Video Intercom with ExacqVision

This article applies to the Axis I8116-E Network Video Intercom using firmware 11.8.66. ExacqVision does not currently support SIP calling functions. However, this device can be integrated for interactive operation with ExacqVision as detailed here. In the example that follows we will step through an example scenario wherein pressing the door station call button brings… Continue reading Using the Axis I8116-E Network Video Intercom with ExacqVision

Using the Axis A8207 Door Station with exacqVision

This article applies to the Axis A8207-VE and A8207-VE MkII Network Video Door Stations using firmware 11.5.64. exacqVision does not currently support SIP calling functions. However, these door stations can be integrated for interactive operation with exacqVision as detailed here. In the example that follows we will step through an example scenario wherein pressing the… Continue reading Using the Axis A8207 Door Station with exacqVision

Audio Inputs and Outputs

For those with a desire to listen to audio or utilize two-way audio to speak to those on site, follow along to learn about configuring your ExacqVision audio inputs and outputs, whether they are analog devices connected directly to your server or IP devices connected across your network.

Exacq Mobile 3 Microphone Support

Microphone support, for sending audio from your device to an exacqVision Server, was added in Exacq Mobile 3, version 8.4. All installations of Exacq Mobile 3 acquired from Google Play and the Apple App Store support sending audio to an exacqVision Server. <br> Important Note To send audio to an exacqVision Server using the mobile… Continue reading Exacq Mobile 3 Microphone Support