Azure Active Directory supports the LDAP interface when properly configured, and therefor LDAP can be used to sync the ExacqVision software stack with the Azure AD instance. Background Information: Lightweight Directory Access Protocol (LDAP) is an application protocol for working with various directory services. Directory services, such as Active Directory, store user and account information,… Continue reading ExacqVision Server and Client support LDAP authentication with Azure Active Directory
Tag: Troubleshooting Active Directory Error Messages
Enterprise Manager supports LDAP authentication with Azure Active Directory
Azure Active Directory supports the LDAP interface when properly configured, and therefor LDAP can be used to sync the ExacqVision Enterprise Manager software with the Azure AD instance. Background Information: Lightweight Directory Access Protocol (LDAP) is an application protocol for working with various directory services. Directory services, such as Active Directory, store user and account… Continue reading Enterprise Manager supports LDAP authentication with Azure Active Directory