Trigger Inputs and Alarm Outputs

Dive into understanding how trigger inputs and alarm outputs work. Become familiar with TTL logic and how to configure devices such as switches or buttons, door contacts, or PIR motion sensors as inputs or triggering outputs to activate lights or more based on events or user input. Trigger Input and Output Alarms help you utilize… Continue reading Trigger Inputs and Alarm Outputs

Using IQeye Input Triggers

When a digital input is triggered on an IQeye camera, the camera transmits a single alarm to indicate the condition. This means that the triggered state cannot be seen on exacqVision Client’s Trigger Input page. To test IQeye digital inputs, you must use them with Event Linking or Event Monitoring. <br>