Using Panasonic Input Triggers

When a digital input is triggered on a Panasonic camera, the camera transmits a single alarm to indicate the condition. This means that the triggered state cannot be seen on exacqVision Client’s Trigger Input page. To test Panasonic digital inputs, you must use them with Event Linking or Event Monitoring. < br>

Trigger Inputs Do Not Work on Panasonic Cameras Running H.264 or MPEG-4 in Internet Mode (Over HTTP)

When a Panasonic camera is configured for Internet mode (over HTTP) when using H.264 or MPEG-4 compression, the camera’s trigger inputs do not work correctly. The triggers are in a normally open state by default, but they do not enter an alarm state when the circuit is closed. <br>