Linux – Delete Video from Root Volume

Exacq Technologies does not recommend using the root partition for video recording as the OS is installed on this partition.  Exacq labels the root partition as /mnt/edvr/0.  In the event that /mnt/edvr/0 has been enabled on the storage page,  resulting in video being recorded to the root partition and you now need to delete that… Continue reading Linux – Delete Video from Root Volume

Adding Desktop Trash Bin in Ubuntu

Steps below are separated by version. To find your version, open a Terminal CLI using the Menu bar, or pressing CTRL+ALT+T. Enter one of the following commands will display your version information. <br> Ubuntu 18.04 & 20.04 <br> Ubuntu 14.04 & 16.04 <br> Ubuntu 12.04 <br> Ubuntu 10.04 <br> Ubuntu 8.04 <br>