Categories
Knowledge Support Video Library Demo Support exacqVision Enterprise exacqVision Client exacqVision Server exacqVision Mobile exacqVision Webservice Categories exacqVision Hardware Products

2021-03 March Quarterly Release Training

Feature – Axis Body Worn Cameras

  • Client – Enhancement – Axis body worn camera support. #21843
  • Client – Enhancement – Added support for search only cameras and audio for Axis body worn.
  • Client – Enhancement – Added config options for axis body worn cameras.
  • Server – axisbwpi – Add support for the Axis body worn camera system #21204

Feature – Large Blobs

  • Client – Enhancement – Support Large Blobs. #21842
  • Server – Enhancement – streampi – Support for maps and other blobs of sizes exceeding 2MB #18412

Client

  • Enhancement – Automatically create a system event linkage for source groups in event monitoring. #22396
    • User will be warned if trying to delete an automatically created Event Link
  • Enhancement – Allow selecting multiple files at once in Add Person #21332
  • Enhancement – Updated Immervision libraries for newer camera model support. #22384
  • Enhancement – Upgraded Oncam dewarping library for newer camera support. #21914
  • Enhancement – Added Linux x64 support for Oncam dewarping. #21914
    • Windows and Linux only
    • Mac library not ready
  • Enhancement – Enterprise LDAP: enable local user accounts checkbox if connected as a local user AND local user accounts are disabled #21933
  • Enhancement – For enterprise and system LDAP pages, disable the option to disable local user accounts if current use is local #21933
  • Enhancement – Added timeout message to export log if we timed out waiting for system or audit logs during support export. #22417
    • If cancelled, then the next export wouldn’t include the Server logs.

Server

  • Feature – rtspserverpi – Add support for video search #20747
  • Backend search capabilities without needing to use our API.
    • Primarily for future projects.
  • Enhancement – AxisPI – Support events for Axis Fence Guard #22465
    • Similar to Line Cross.
    • Must be configured in the camera with a browser.
  • Enhancement – AxisPI – Improve performance of downloads from edge storage #22303
    • 5m sub-operations to split up data and better protect against lost video due to network disconnection.
    • Parallel downloads – Off by default, must be configured.
  • Enhancement – AxisPI – change to more efficient log format #22502 §Similar to Onvif/Illustra
  • Enhancement – Illustra3pi – Correctly identify Holis cameras #22222
    • Some were improperly added from the scan as Onvif before.
    • Still using the Illustra3 plugin but will show up in the Client as Hollis.
  • Enhancement – onvifnvcpi – Add Support for Vivotek MA9321/2-EHTV #22373
    • Other json updates for specific cameras as well.
  • Enhancement – onvifnvcpi – Add the Subscription Renew command to pullpoint if MaxNotificationProducers capability is detected. #22165
    • Resolves some of the “Motion not supported” messages.
  • Enhancement – onvifnvcpi – Add override for cameras that prefer GetCapabilities instead of GetServices. #20941
  • Enhancement – plugins – hardened config persistence against unexpected shutdowns #15944
    • Changes in how config file gets edited and saved.
      • *.xml.bak created first
      • Changes saved to *.xml.pending
      • *.xml.pending then renamed to *.xml
    • Changes in how config files are loaded.
      • *.xml.pending is always most recent save. Load it first
      • Then try *.xml
      • Then try *.xml.bak
    • log load/save errors for core.xml.

Web Service

  • Enhancement – Add ability to monitor and remove temporary files. #22276
    • Thumbnails and Search results
    • Now cleaning up after 12 hours.
  • Enhancement – Add RTSP URI to camera endpoint. #22568
    • API feature – no UI
    • Will be utilized by Integrations
  • Enhancement – Sort available update versions, newest first. #18059

Enterprise Manager

  • Enhancement – Made licensing page more responsive #19096
  • Enhancement – Added filter to add user group lists #22528
  • Enhancement – Added extra server fields to server detail and list pages #19153