Server Enhancement – core, LogPI – allow to dynamically control logging level per plugin #19954Enhancement – itv2pi – Add more verbose logging and debug logging to help troubleshoot issues in the fieldEnhancement – streampi – Adding logging to help troubleshoot LDAP binding issuesEnhancement – rtspserverpi – plugin to provide rtsp stream from server. #19100Feature –… Continue reading 2019-12-09 – December 2019 Quarterly Release Training
Tag: Training
2019-09-10 – September 2019 Quarterly Release Training
Client Enhancement – Added RTSP server configuration page. ›Still requires – Server-side work.Enhancement – Added AutoGroups to automatically populate groups based on attributes assigned for cameras and/or systems. – #18433Enhancement – Advanced filtering for camera and system metadataEnhancement – Password fields no longer auto populate.Enhancement – Added support for dynamic camera plugin settingsEnhancement – Added… Continue reading 2019-09-10 – September 2019 Quarterly Release Training
2019-06-11 – June 2019 Quarterly Release Training
Client Enhancement – Added option to enable POS database encryption. #18660Enhancement – Re-enable GPU decoding on macOS 10.14 and higherEnhancement – Added support for newer Bosch fisheye models and firmware. #14843Enhancement – Ptz/Digital Ptz presets can now be saved from live modeEnhancement – Enable GPU decoding for G-Series and G-Series PoE systems. ›Enhancement – Refactor… Continue reading 2019-06-11 – June 2019 Quarterly Release Training
2019-03-13 – March 2019 Release Training
Server-side Versioning scheme changedAdditional executables moved to ‘exacqd’ (SCN) – ArchivePI, NetworkStoragePI, SysmgmtPIAxis VMD4 configurationSamsung plugin now supports Video BackfillSamsung sound and object IVA analytics now supported (up to 7)Network configuration work for Ubuntu 18.04, networkdLinux core dumps now in logs folder – Dumps still disabled by default (Internal KB 16376) – Only one dump… Continue reading 2019-03-13 – March 2019 Release Training
2018-09-05 – Quarterly Release Training 9.6
Server 9.6 EdgeStor (Network Loss Recording) – NOT RELATED TO “exacqVision EDGE” – Requires configuration in the camera’s webpage – Requests video stored on Camera’s SD card – Video converted to PS file – Axis and Illustra so far – Not a separate plugin, included as part of the IP Camera plugin. – Video may… Continue reading 2018-09-05 – Quarterly Release Training 9.6