2024-09 September Quarterly Release Training

<br> exacqVision Server exacqVision Client exacqVision Web Service exacqVision Enterprise Manager Exacq Mobile 3 exacqVision Mobile Exacq Hardware Hardware Revisions exacqVision Advantage Illustra <br>

2024-03 March Exacq Release Training

This training covers the following topics: Quick Add – Requires exacqVision Server and Client 24.03 or higher. Supports only Illustra Flex and Pro Gen 3/4 cameras. Architecture changes – Changes made in how the new exacqVision Mobile app connects to exacqVision Server and when exacqVision Web Service is still required. Remote Connectivity – Provided for… Continue reading 2024-03 March Exacq Release Training

2023-09 September Quarterly Release Training

<br><br> ExacqVision Server Bug Fix – Fixed issue causing server crash due to missing microSD card in Illustra multisensor cameras.If camera has no microSD for one sensor, but does for another, network loss recording action caused a crash. (AESW-7549) Bug Fix – Prevent offload from Illustra BWC from hanging Bug Fix – If camera does… Continue reading 2023-09 September Quarterly Release Training

2023-06 June Quarterly Release Training

ExacqVision Server Bug Fix – Fixed excessive Archiving status messages (AESW-4989) Bug Fix – Debian installer no longer enabled eventpi by default Bug Fix – Fixed issue capturing all metadata when multiple events are sent as one alarm Bug Fix – Ensure eventpi database is purged after server reboot Bug Fix – Fixed connection status… Continue reading 2023-06 June Quarterly Release Training

2023-03 March Quarterly Release Training

ExacqVision Server Bug Fix – Fixed PTZ preset administration for custom users to create presets for analog cameras (AESW-4357) Bug Fix – Fixed monitoring RAID background tasks, like consistency checks and background initialization (AESW-4387) Bug Fix – Fixed reporting incorrect RAM, was displaying MB instead of GB (AESW-2498) Bug Fix – actipi – Reduce metadata… Continue reading 2023-03 March Quarterly Release Training

2022-12 September Quarterly Release Training

ExacqVision Server Bug Fix – Fixed issue preventing archiving of analog video to Cloud Drive Bug Fix – Motion Detection not working on Holis cameras Bug Fix – Corrected issue setting NTP server for illustra3pi and illustramultipi camera plugins Bug Fix – Fixed issue with missing frames from PTZ cameras causing image tearing in recorded… Continue reading 2022-12 September Quarterly Release Training