Are DSCP/ToS set in exacqVision Server/Client Packet Headers

Title Are DSCP/ToS set in exacqVision Server/Client Packet Headers Description  exacqVision Server/Client packets do not utilize DSCP/ToS (Differentiated Services Code Point (DSCP) Type of Service (Tos). Product  exacqVision ServerexacqVision Client Description  The ToS (type of service) or DiffServ (differentiated services) field in the IPv4 header, and the Traffic Class field in the IPv6 header are… Continue reading Are DSCP/ToS set in exacqVision Server/Client Packet Headers