Toggling a Web Service Connection Multiple Times Can Cause Failed Initialization

Description Enabling and then Disabling a Web Service multiple times within Exacq Mobile 3 during the connection process can prevent the servers from being retrieved. <br> Version Introduced <br> Platform Mobile-All <br> Steps to reproduce <br> Expected result The Server List is displayed <br> Actual result The Text ‘Unable to retrieve servers’ is displayed <br>… Continue reading Toggling a Web Service Connection Multiple Times Can Cause Failed Initialization