Exacq Mobile 3 app does not allow cameras to show Time stamps OSD of the server time while in a different TIME ZONE than the recorder

Description  The Exacq Mobile 3 application does not show the OSD of cameras while the device is in a different time zone. Product  Exacq Mobile 3 application for both iPhone and Android. Expected Results  We should be able to account for when the Device is in a different time zone than the recorder while using… Continue reading Exacq Mobile 3 app does not allow cameras to show Time stamps OSD of the server time while in a different TIME ZONE than the recorder

Onvif plugin now supports camera timestamping

The Onvif plugin has always time-stamped frames as they arrive at the server. With issues of network latency and camera streaming problems, this could cause video to look jittery. An option was added to provide time-stamping with camera time. Adding #timestamp=camera in the hostname would use the presentation time provided by the camera. The default… Continue reading Onvif plugin now supports camera timestamping

Incorrect Timestamps

Issue: exacqVision Server may cause incorrect frame timestamps for some cameras that are using RtspPI or AxisPI plugins. Workaround: None Version Affected 20.06.4 and earlier Resolution: A new Override is available for RtspPI and AxisPIThe Override will prevent the server from auto adjusting timestamps and will trust verbatim what comes from camera. The server generates… Continue reading Incorrect Timestamps

ESM Event Timestamp Incorrect After Time Zone Change

If you change the time zone on a system running Enterprise System Manager (ESM), the timestamp of ESM events might not match the time that the events actually occurred. <br> When ESM services are started, ESM reads the timezone configured in the operating system. If the system’s time zone is then changed, you must restart… Continue reading ESM Event Timestamp Incorrect After Time Zone Change

Using Antivirus Software with exacqVision

Antivirus Configuration As with all third-party software not on the Product Integration section, the user assumes the risk of software incompatibility with the exacqVision software suite. To permit antivirus software to work with exacqVision software, the following file extensions need to be exempted from scans: NOTE: As an alternative, you could also exclude the data drive you… Continue reading Using Antivirus Software with exacqVision

exacqVision Timestamp Format

All exacqVision video is timestamped in UTC, so there is no ambiguity as to the absolute time when the video was recorded. When exporting video, the time zone of the system on which the video was recorded is not stored. Starting with exacqVision version 3.4, two features were added to make this more transparent to… Continue reading exacqVision Timestamp Format