From the administrative instances manager (https://admin.exacq.net/instances.php) locate the desired instance In the Actions drop down menu select,Update ESM and choose the desired time zone in the Select a time zone drop down menu and click Okay
Tag: Time Zone
Time Zone Only Shows UTC-0 Option
Symptom In the exacqVision Client software on the ‘System Configuration’ page, under the ‘Date/Time’ tab, the Time Zone drop down menu has only one option, UTC-0. <br> Problem The user cannot set the proper server time zone. Affecting only Windows systems, the script that obtains the time zones from the operating system has failed. The… Continue reading Time Zone Only Shows UTC-0 Option
exacqVision Edge Time Zone Configuration
exacqVision Edge is a version of exacqVision Server that runs directly on supported camera models and only connects to, and records video from, the camera it is hosted on. Cameras running the exacqVision Edge, or Edge+, application must be configured for the GMT+0 time zone. Because the server application runs directly on the camera, the… Continue reading exacqVision Edge Time Zone Configuration
Time Settings and Time Zone Information
Background Information The Windows or Linux (Ubuntu) operating system time of your exacqVision Server host should be set to the local time and time zone where it is located. It is often desirable to synchronize the system to a central time server, rather than rely on the internal clock of the recording server. There are… Continue reading Time Settings and Time Zone Information