Incorrect Timestamps

Issue: exacqVision Server may cause incorrect frame timestamps for some cameras that are using RtspPI or AxisPI plugins. Workaround: None Version Affected 20.06.4 and earlier Resolution: A new Override is available for RtspPI and AxisPIThe Override will prevent the server from auto adjusting timestamps and will trust verbatim what comes from camera. The server generates… Continue reading Incorrect Timestamps

Camera Time Stamp Off by Years

Some cameras, particularly AXIS and Sony models, display an OSD date with an incorrect year. The time and date of the camera might be set to GMT and the Windows time is correct on the server, yet the OSD on the screen shows something like March 2, 2001. <br> This is usually a result of… Continue reading Camera Time Stamp Off by Years