Configuring the Time Server on Linux-based exacqVision Systems

To configure the time server on a Linux-based exacqVision system, complete the following steps: In exacqVision Client, make sure Enable Time Server is not selected on the Date/Time tab on the System Setup page.In a Terminal window, type sudo /etc/init.d/edvrserver stop to stop the exacqVision service.In a Terminal window, type sudo /etc/init.d/ntp start.Type sudo /etc/init.d/edvrserver… Continue reading Configuring the Time Server on Linux-based exacqVision Systems