Description Video is not being recorded for cameras scheduled to record on Time Lapse when running exacqVision Server version 22.12. 3.0 Product ExacqVision Server version 22.12.3.0 Steps to Reproduce Update from earlier version of exacqVision Server to 22.12.3.0Search for time lapse recorded video any time after the update Expected Results Video results are returned and… Continue reading Time Lapse Recording Broken in exacqVision Server 22.12.3.0
Tag: Time Lapse
Time Lapse Capture an Image Reverts Back to 1 Second in the Drop Down Menu
Description When selecting a Time Lapse under the cameras settings page in the client, Click Set, then hit the apply in the lower left. Once that happens the Box for the seconds/minutes/hours will revert back to 1 seconds. Product Server/Client Time Lapse Expected Results In the drop down box if you select 5 seconds and… Continue reading Time Lapse Capture an Image Reverts Back to 1 Second in the Drop Down Menu
H.264 Camera Configuration for Time-lapse Recording
H.264 compression uses a Group of Pictures (GOP) or Group of Video (GOV) to define how many P-frames are sent between each I-frame. (I-frames are complete pictures, whereas P-frames are partial frames reconstructed based on the last I-frame and all the P-frames in between.) Time-lapse recording stores I-frames. If time-lapse recording is configured at short… Continue reading H.264 Camera Configuration for Time-lapse Recording