Description
In exacqVision Server versions 21.09 and 21.12 if audio outputs or push to talk are used it can cause a slow memory leak every minute. This will eventually cause the server to throttle and eventually hang or reboot.
Product
- exacqVision Server 21.09
- exacqVision Server 21.12
Solution
Upgrade exacqVision Server to RC 21.12.3 or higher, which contains enhancements which should resolve the issue.
12/08/2021
v21.12.1
- Enhancement – psfpi – Throttle audio as well as video when the system is throttling.
01/14/2022
v21.12.3
- Bug Fix – psfpi – Changed to time based cache rather than packets to address an issue related to push to talk
<br>