When troubleshooting TCP/IP connectivity issues, it is often helpful to confirm that the network path is open over a specified port and that there is no interference from a firewall or antivirus. This also rules out software level problems that may be causing a failure to connect. While there exists many utilities to accomplish this… Continue reading PortCheck Utility
Tag: Test
exacqVision Hard Drive Tests
Description A summary of system drive tests performed by exacqVision using evSelfTest, RAID controllers, and S.M.A.R.T. data. Product Information On systems Built-by-Exacq (BBE), the exacqVision software runs the following tests: Using evSelfTest.exe: RAID card consistency check, once every week.On non-BBE systems:
Enterprise System Manager Shell
To open Enterprise Manager Shell in Windows, run Command Prompt as an administrator and change directories to the installation directory by running the following command: cd C:\Program Files\exacqvision\enterprisemanager \enterprisesystemmanager\ Then type: enterprisesystemmanager.exe shell To open Enterprise Manager Shell in Linux, open a Terminal window and type: sudo /usr/local/exacq/esm/enterprisesystemmanager shell <br> The following commands can be used… Continue reading Enterprise System Manager Shell
How to Test an ATX Power Supply
Although there are portable power supply testers on the market that are inexpensive, it often becomes necessary to test whether a power supply is good or bad with only a multi-meter handy. The following steps detail how to perform this. <br> WARNING: When working with electricity always follow proper safety procedures. Remove jewelry from your… Continue reading How to Test an ATX Power Supply