Symptom Client displays temperature alarms on hard drives. These may indicate temperatures near 1° C, or between ~20000-30000° C. <br> Problem This behavior was seen from the following Western Digital HD models when connected to LSI storage controllers. WD4002FYYZWD8002FRYZWD8003FRYZWD6002FRYZWD80PUZXWD101KRYZWD121KRYZ <br> Solution Update the ExacqVision Server version to 9.3.9 or higher, also back-patched into 9.2 RC. <br>