Description Some Exacq hybrid systems built since 7/23/2024 and running Ubuntu 22.04 have exhibited a freeze of the analog video after running for some period of time. This is likely a result of a false-positive error state in the PCIe ASPM (Active-state Power Management). This can be confirmed using a Terminal with the following command:… Continue reading Analog video freezing on tDVR 8016e capture boards – Linux
Tag: tDVR
TDVR Capture Card Faulty Board
Description There were reports of capture cards working for upwards of 10 minutes and then would fail to produce video in live views. We have identified the issue and made the proper corrections. If this is seen on a system please follow the instructions below to identify if the board is affected. Then take the… Continue reading TDVR Capture Card Faulty Board
Who manufactures Exacq video capture boards?
Exacq designs and manufactures its own video capture boards. Current tDVR capture board models are manufactured in Canada. Previous eDVR and sDVR capture boards, no longer manufactured, were designed by Exacq. Portions of the manufacturing process were performed by a contract manufacturer. <br>