On certain exacqVision A Series and Z Series systems, faulty memory causes the system to restart and causes the Windows exacqVision Client to crash (if VGA Acceleration Mode enabled). The following procedure can determine whether the affected memory is installed on a system: <br> WINDOWS Log in to Windows as an administrator.Select the Start menu… Continue reading Bad Memory Causes exacqVision Client Crash and System Reboot