ASRock Industrial IMB-X1314 System Beep Codes

Beep SequenceDescriptionTroubleshooting1 short constant beepError with RAM refresh1. Check RAM for physical damage.2. Try another stick of RAM.3. BIOS update2 short beepsRAM parity error1. If adding new memory, try removing to see if this fixes issue.2. Check for conflicts in memory types.3. Check power supply for unstable voltages.3 short beepsRAM read/write test failed1. Repair corrupted… Continue reading ASRock Industrial IMB-X1314 System Beep Codes

ASRock Industrial IMB-X1313 System Beep Codes

Beep SequenceDescriptionTroubleshooting1 short constant beepError with RAM refresh1. Check RAM for physical damage.2. Try another stick of RAM.3. BIOS update2 short beepsRAM parity error1. If adding new memory, try removing to see if this fixes issue.2. Check for conflicts in memory types.3. Check power supply for unstable voltages.3 short beepsRAM read/write test failed1. Repair corrupted… Continue reading ASRock Industrial IMB-X1313 System Beep Codes

ASRock H410 System Beep Codes

Beep SequenceDescriptionTroubleshooting1 short constant beepError with RAM refresh1. Check RAM for physical damage.2. Try another stick of RAM.3. BIOS update2 short beepsRAM parity error1. If adding new memory, try removing to see if this fixes issue.2. Check for conflicts in memory types.3. Check power supply for unstable voltages.3 short beepsRAM read/write test failed1. Repair corrupted… Continue reading ASRock H410 System Beep Codes

ASRock C236M WS System Beep Codes

Beep SequenceDescriptionTroubleshooting1 short constant beepError with RAM refresh1. Check RAM for physical damage.2. Try another stick of RAM.3. BIOS update2 short beepsRAM parity error1. If adding new memory, try removing to see if this fixes issue.2. Check for conflicts in memory types.3. Check power supply for unstable voltages.3 short beepsRAM read/write test failed1. Repair corrupted… Continue reading ASRock C236M WS System Beep Codes

ASRock H110-E1 System Beep Codes

Beep SequenceDescriptionTroubleshooting1 short constant beepError with RAM refresh1. Check RAM for physical damage.2. Try another stick of RAM.3. BIOS update2 short beepsRAM parity error1. If adding new memory, try removing to see if this fixes issue.2. Check for conflicts in memory types.3. Check power supply for unstable voltages.3 short beepsRAM read/write test failed1. Repair corrupted… Continue reading ASRock H110-E1 System Beep Codes

Asus Q87-MA System Beep Codes

Beep SequenceDescriptionTroubleshootingOne short beepNormal bootOne short beep, nothing displays on monitorNormal bootCheck that the monitor is functioning and connected correctly.Power light is ON, no beepHardware issueCheck that the CPU and memory are installed correctly and there is no corrosion or dirt on the connections.One continuous beep followed by two short beeps, then a pause (repeating)No… Continue reading Asus Q87-MA System Beep Codes

Enabling both HDMI and VGA via the BIOS

Description  How to configure an ASRock system board if HDMI Output has been lost and both HDMI & VGA monitors are being used.   Product  Steps to Reproduce  Expected Results Both monitors display video  Actual Results Video is lost on both monitors  Solution

Audio from motherboard sounds “choppy”

Description Users report “choppy” audio from motherboard audio outputs on Linux-based systems. <br> Affected platforms exacqVision Server 5.8 to 7.2.3, on Linux systems <br> Symptom Sound quality of audio coming from motherboard sounds “choppy”. <br> Workaround No workaround <br> Resolution Update to exacqVision Server 7.4.0.89244 or higher

Motherboard audio continues to play even after disabling the audio channel

Description Audio coming from outputs on motherboard continues to play even after disabling the audio channel. <br> Affected platforms exacqVision Server 5.8 to 7.2.3 <br> Symptom Motherboard audio continues to play the buffered sound on the output port even after the port is disabled from exacqVision client. <br> Workaround Restart the exacqVision service <br> Resolution… Continue reading Motherboard audio continues to play even after disabling the audio channel