Description: If navigating from one suspect tracking area to another we found that the button for that next camera is not sustaining. You have to click on the button from the associations again in order to select the next camera to navigate to. Product: Found on Server Version 22.12 and 23.03 Workaround: Close the Client… Continue reading Client Machine Suspect Tracking Button Stops Working
Tag: Suspect Tracking
Camera Settings
Nested in the configuration tree, beneath Camera Recording, is the list of all cameras connected to the system. Clicking on any of these cameras will display the settings page for that individual camera. From here, you have access to important settings, such as the camera name, configuring the optional on-screen display (OSD), picture settings, motion… Continue reading Camera Settings
How to Configure Suspect Tracking
How to configure suspect tracking Introduced in exacqVision 8.0, suspect tracking provides users with a visual method of following a person or object moving through several camera scenes. Suspect tracking is featured as a new tab on the camera settings page. If you already have cameras laid out on a map that includes the camera… Continue reading How to Configure Suspect Tracking