Setting up Illustra3 camera for https support in 8.4.1 server.
<br>
- All Illustra3 devices(Pro/825/625/mini-dome/mini-bullet/2mp LTĀ Pro/Flex?) should all factory defaulted to both(http/https) modes with self signed cert.
- 8.4.1 server will ONLY support all Illustra3 devices in both(http/https) mode.
- To upload a cert file, log onto the camera web page. The http/https page is either in security or network/advanced settings page depends on fw.
- Connect camera with server 8.4.1 and the lock will indicate HTTPS connection.
- Only configuration is encrypted not the streams.