Native Streaming in the Web Client

Affected platforms exacqVision 7.2 or later <br> Description exacqVision 7.2 introduces native h.264 video streaming to the web client. When a browser session connects to the web service, the browser and web service negotiate whether transcoding or native streaming will be used. The following logic describes how this is negotiated: If the browser does not… Continue reading Native Streaming in the Web Client

Axis showing “Request Not Found” when streaming video

Description When connecting to some Axis cameras that do not support shock event, it could get into a state showing “Request Not Found” in the status of “Add IP Cameras” page. When in this state, the camera is actually connected and streaming video. The issue is that the device does not support shock returning a… Continue reading Axis showing “Request Not Found” when streaming video

Panasonic 360-degree Network Camera Multistreaming

Panasonic 360-degree network cameras can send up to three streams to exacqVision. This includes one JPEG stream, and two H.264 streams. All three streams are configured on the same page in the camera’s web configuration page. If you configure two additional streams on the camera in exacqVision Client, either the main stream or one of… Continue reading Panasonic 360-degree Network Camera Multistreaming