Video Codecs vs Video Containers

CodecsCodec is a term that combines compression and decompression. Transmitting video streams or storing video files in a compressed format to save bandwidth and storage capacity requires one algorithm to compress the video and another to decompress it at the system receiving the stream or playing the file. Containers Containers are just that, a container… Continue reading Video Codecs vs Video Containers

Axis with VMD4 reporting “Device reporting an error” and stream video

Description This is limited to Axis cameras supporting VMD4 (fw 6.50 and later) either after factory default or out of box. In this case, the plugin detects VMD4 is preferred over VMD1 and by default VMD4 is stopped. The Axis plugin in this case sends a request to start VMD4 and some camera model and… Continue reading Axis with VMD4 reporting “Device reporting an error” and stream video