ExacqVision Hard Drive Self-Test Options

Title ExacqVision Hard Drive Self-Test Options Description  Differences between short and log self-tests performed on hard drives for BBE systems. Product  ExacqVision Server Information Short Test Test electrical properties of drive(s)Test mechanical properties of drive(s)Complete a read and verify test on some sectors of drive(s) Long Test Test electrical properties of drive(s)Test mechanical properties of… Continue reading ExacqVision Hard Drive Self-Test Options

False Positive drives offline status for disks labeled “sat” – invalid disk type errors

False Positive drives offline for disks labeled “sat” – invalid disk type errors Exacq Support has identified an issue with SMART attribute labels causing false positive drive offline errors on the hardware tab of ExacqVision Client. Some Disks may show error of “invalid disk type”   Some systems may contain drives that get listed as… Continue reading False Positive drives offline status for disks labeled “sat” – invalid disk type errors

For Debugging Purposes, The Logging of Additional Information Related to the Storage Self-Tests May Be Enabled.

Starting with server version 19.08, it is now possible to collect additional information about storage self tests. evselftestYYYY-MM-DD.txt files in the server/logs path will trace all of the commands that evselftest issues along with their corresponding output. This feature is turned on when the EvselftestLogEnabled attribute under “Storage” is set to “1” in sysmgmtpi.xml.