Affected Versions exacqVision Server 7.6 and earlier <br> Description The server will crash on start-up if the audit directory does not exist and the server cannot create a valid audit directory. An example of this is when ‘audit’ is a symlink with an invalid target or a file exists with the same name as the… Continue reading Server crashes on start-up when audit directory cannot be created
Tag: Startup Crash
Server crash on start-up with 9.8.2
Symptom: System enters a crash loop after running for some time on Windows platforms. Problem: This issue is caused by a handle leak and manifests itself as a networking error or failure to create processes. Logs may indicate the following: 1/9/2019 3:12:25 AM StreamPI Warning LDAP: Failed to execute (1450). 1/9/2019 3:12:25 AM StreamPI Warning… Continue reading Server crash on start-up with 9.8.2