If you are using Internet Explorer 8 to connect to an S2 access control system integrated with exacqVision, a “Stack overflow error 0” message might appear repeatedly. This issue occurs more often if the S2 and exacqVision systems are connected on the same LAN, and it is caused by the way Internet Explorer 8 handles… Continue reading Stack Overflow in S2 Integration in Internet Explorer 8