Using Rsync to Transfer Files to a Cloudvue Gateway

Description  At times it may be necessary to move files to a Cloudvue Gateway and while other tools such as SCP or MobaXterm can usually manage the job, rsync can track progress and resume after an interruption which can be particularly useful when transferring large files like the latest Cloudvue software or on slow or… Continue reading Using Rsync to Transfer Files to a Cloudvue Gateway

Adding an Authorized Public SSH Key to a C2C

Description  SSH access to Cloudvue C2C devices  depends  on  RSA public/private key pairs.  Public keys for L3 Cloudvue support were added into the Cloudvue production software with the release of 22.9.0 in January of 2023.   The following instructions can be used to temporarily add a public ssh key to a C2C device.  SSH public keys… Continue reading Adding an Authorized Public SSH Key to a C2C

Moving Files From Cloudvue Gateway to Windows

Description  At times it may be necessary to move or copy files from a Cloudvue Gateway to a local machine. WinSCP Portable establishes an SSH  connection between a machine running Windows and a Gateway.  It offers a convenient side by side file explorer view of the local and Gateway directories and files making it simple to… Continue reading Moving Files From Cloudvue Gateway to Windows

Manually Calculating the SSH Password for a Cloudvue Device

*** INTERNAL USE *** Description  The following instructions can be used to manually calculate the ssh password for a Cloudvue video device. Product  Solution Cloudvue Gateway The ssh password is the first 32 characters of the MD5 Hash returned when using the following combination MAC + Version + 3cadcddd84a94e1014f6a9bfeeecfd6 Where MAC is the MAC address… Continue reading Manually Calculating the SSH Password for a Cloudvue Device

Enabling / Disabling SSH on ExacqVision Linux Server

Description  SSH is installed on ExacqVision Servers at the time of manufacture; however, for security purposes, SSH is disabled.  To enable remote administration of your ExacqVision system via SSH, it must first enabled.  Product  Linux (Ubuntu) Solution Using Exacq Linux Utilities  Using scripts To Enable To Disable  Installing the Package Using Terminal To Enable sudo… Continue reading Enabling / Disabling SSH on ExacqVision Linux Server