Skip to content

Exacq

Support Portal CMS

Tag: Sound Cards

The audio is not working and showing “PA_OpenStream (-9996) Invalid device”

Description The audio is not working on the Exacq server and is giving a message “PA_OpenStream (-9996) Invalid device.” Solution The issue is a failed sound card, so it needs an RMA to replace the motherboard or install another sound card

Published April 3, 2023
Categorized as Knowledge Support, Support, exacqVision Hardware Tagged Hardware Issues, Public, Sound Cards, 14036

Soundpi Does Not Detect Some Sound Cards on Linux

Problem: System audio is not listed in client because soundpi does not detect some sound cards in Linux. Introduced in Server 8.9.6.  <br> Solution: Update to Server 9.2.x

Published April 27, 2021
Categorized as Knowledge Support, Support, exacqVision Server, Categories, Products Tagged Linux, Level2, soundpi Does Not Detect Some Sound Cards, Sound Cards, SoundPI, 4881

Recent Posts

  • Synchronize with Enterprise Manager authentication – Connectivity error:500
  • Exacq Mobile Application Views show Black Box
  • Using an Axis D3110 Connectivity Hub with the Axis C1410 MK11 Speaker
  • FLIR Camera Motion Stops Recording Motion Events
  • exacqVision 25H1 Release Bulletin