Jagged Edges Appear on Sony SNC-HM662 Using Third Party Dewarper

Description  When using the Immervision dewarper on the Sony SNC-HM662 jagged edges will appear in the live view of the camera. Product  Any ExacqVision NVR Steps to Reproduce  Expected Results  You are able to utilize DPTZ with no issues Actual Results  Jagged edges appear around the camera’s view Solution The issue resides on the third… Continue reading Jagged Edges Appear on Sony SNC-HM662 Using Third Party Dewarper

Sony generates excessive configuration events with invalid ntp server

Description sony generates excessive configuration events with invalid ntp server <br> Version Introduced v3.3.3.15350 <br> Steps to reproduce enable an ip camera time server override with characters requiring url encoding <br> Expected result time server override value is set in camera <br> Actual result plugin continuously fails to update camera <br> Work Around configure the… Continue reading Sony generates excessive configuration events with invalid ntp server

IP Plugin Overrides

The standard form for exacqVision camera addresses is as follows: {host}{?parameter_1=value_1}…{?parameter_n=value_n}{#override_1=value_1}…{#override_n=value_n} <br><br> Overrides PluginOptionUsageACTitransport=httpHTTP stream support for legacy platforms and user dataACTitransport=rtspRTSP stream with separate metadata socket for motion/input trigger/video loss/etc.Axiszoom=configBy default zoom only cameras support.Axiszoom=operationForce zoom only operation and controls as part of PTZ and live view.Axisblocksize=offOn by default, but could turn off blocksize… Continue reading IP Plugin Overrides

Camera Time Stamp Off by Years

Some cameras, particularly AXIS and Sony models, display an OSD date with an incorrect year. The time and date of the camera might be set to GMT and the Windows time is correct on the server, yet the OSD on the screen shows something like March 2, 2001. <br> This is usually a result of… Continue reading Camera Time Stamp Off by Years