Solr Apache API on port 8983

There is currently a fix for customers who are able to access the Solr Apache API admin page from a workstation. Download EM version 21.12.2 and install it. If you are still able to access the Solr Apache API admin page on a workstation that is not the local NVR hitting port 8983, it is… Continue reading Solr Apache API on port 8983

Enterprise Manager Updating Java Version in Solr

Issue Enterprise Manager uses a package called Solr which in turn uses Java.  Currently, we do not offer an update path for Solr that will update the Java version.  The following instructions can be used if the need arises were Java needs to be updated.   Resolution Windows 64-bit Assumes EM is installed at C:\program files\exacqVision\EnterpriseManager for Windows 64 bitDownload… Continue reading Enterprise Manager Updating Java Version in Solr