Internal Resources Configuration Calculator Platform: AllThis web-based utility was intended as a Sales tool, but can be utilized for troubleshooting to determine if machines are over-taxxed based upon their current load of cameras. After inputting the customer’s current camera load, you can see the expected data rates at the bottom. Also, the “Compatible Models” on the… Continue reading Common Tools and Resources
Tag: Software
Identifying exacqVision Development Software Versions
Software Continuing changes to exacqVision software follows a standardized version control system which allows for quick identification of the type of build that is being installed. Software is numbered by a 4-part system as follows: [major].[minor].[revision].[build] The first 2 elements will tell you the calendar year and month. Version 23.06.776000.0 was released in the year… Continue reading Identifying exacqVision Development Software Versions
Downgrading Software on Ubuntu/Linux OS
Ubuntu/Linux uses the ‘gdebi’ package installer to run .DEB packages. This will automatically check if you are attempting to install an older package than is already installed and warn you if a newer version is already installed. If you choose to downgrade the version of your ExacqVision Server, Client, or Web Service software you will… Continue reading Downgrading Software on Ubuntu/Linux OS
How do I check the software subscription on my ExacqVision Server?
The following methods allow you to examine a system’s license details and SSA expiration: Using the Systems page (Multiple Systems) Using the Configure System page (Single System) Using the SSA tools on Exacq.com