Alarm Output Soft triggers on Thin Client triggering on and off automatically

DescriptionWhen a Alarm Output Soft Trigger is enabled in the thin client it triggers on and off every 10 seconds automatically. Product Exacq Thin Client Exacq Web Service Steps to Reproduce Setup an alarm output to a soft trigger on exacq Access this soft trigger on the thin client Enable the soft trigger Expected Results Alarm stays on… Continue reading Alarm Output Soft triggers on Thin Client triggering on and off automatically

The Event monitoring trigger is not switching the video

The Event monitoring trigger is not switching the video Description The Event monitoring trigger is not switching the video the first time if you run it while another trigger works. Reproducing the issue:- creating Two event monitoring profiles using the Video Panel/View type and setting two soft triggers to trigger it manually, then set the… Continue reading The Event monitoring trigger is not switching the video

Limited Features available in the Thin Client .

This is not an exhausted list.Soft Triggers are not available in the Web Browser/Thin Client. Customers should use the Exacq Mobile 3 Client from a Web Browser instead. The physical triggers are located in the menu of the mobile browser instead of on the live view. For Example: If you are using a trigger for… Continue reading Limited Features available in the Thin Client .

Using Soft Triggers from CCure 9000 with Event Linking

From the C-Cure 9000 interface, find the Camera ID as pictured below. Setup a “Soft Trigger” under the “Action” tab. Change the “Action Type” to “Soft Trigger. Back in the exacqVision Client, create a new Event Link using the Event Type of “Soft Trigger” and the “Event Source” will match the Camera ID from above.

Configure Event Linking to Include Video in Notifications Triggered by Non-Video Events

Description  Starting with exacqVision 5.10, you can configure email notifications to include a video clip or still image from one or more cameras even if the event does not directly involve video (that is, if the event is not video motion, video loss, IP camera connection, or analytics) using Source Groups to associate video to… Continue reading Configure Event Linking to Include Video in Notifications Triggered by Non-Video Events