Failing email notifications after update to Enterprise Manager version 23.09.9.0

April 4th, 2024 Enterprise Manager may fail to send email notifications after update to 23.09.9.0. ExacqVision support has identified an issue with failing email notifications after updating Enterprise Manager from a previous version to version 23.09.9.0 and up. This occurs when checking “Anonymous” as the send user, or additional configuration required for Exchange servers has… Continue reading Failing email notifications after update to Enterprise Manager version 23.09.9.0

exacqVision Default Ports

Description  The following is a list of default port numbers used by exacqVision software. NOTE: Many ports listed below may only used with certain configurations or by optional services and integrations. Products Port List PortDescription25Simple Mail Transfer Protocol (SMTP)80exacqVision Web Server/exacqVision Enterprise Manager (HTTP)How to change Web Service portsHow to change EM web ports389LDAP (Lightweight… Continue reading exacqVision Default Ports

Sending Notifications With Gmail in Exacq

Description  You can configure an ExacqVision system to use Gmail SMTP Server to send an e-mail notification when an event occurs. Product  ExacqVision Desktop Client Solution Google has announced starting May 30, 2022, They will no longer support the use of third-party apps or devices which ask you to sign in to your Google Account using… Continue reading Sending Notifications With Gmail in Exacq

Enterprise System Manager Shell

To open Enterprise Manager Shell in Windows, run Command Prompt as an administrator and change directories to the installation directory by running the following command: cd C:\Program Files\exacqvision\enterprisemanager \enterprisesystemmanager\ Then type: enterprisesystemmanager.exe shell To open Enterprise Manager Shell in Linux, open a Terminal window and type: sudo /usr/local/exacq/esm/enterprisesystemmanager shell <br> The following commands can be used… Continue reading Enterprise System Manager Shell