Updating the BIOS on Systems with ASRock C236M WS Motherboards

Description  The following instructions can be used to update the BIOS on systems with ASRock C326M motherboards. Product  Asrock C236M WS Motherboard Instructions Download the C236MWS3.12E flash file HEREFormat a 32MB or larger USB key as FAT32Copy the flash file to the root of the USB keyPlug the USB key into the NVR and restart… Continue reading Updating the BIOS on Systems with ASRock C236M WS Motherboards