Summary If you configure a Windows-based computer that has more than one network adapter on the same physical network and protocol subnet, you may experience unexpected results. This article describes the expected behavior of this kind of nonstandard configuration. More Information Consider the following scenario: In this scenario, you may expect the two adapters on… Continue reading How multiple adapters on the same network are expected to behave
Tag: SMB Netowrk
System watchdogs while archiving when SMB network share connection is lost
Affected platforms exacqVision 7.1.23 to 7.2.0 running on Ubuntu Linux <br> Symptom If the recorder is archiving and cannot reach an SMB archive target, the recorder will become unresponsive and watchdog reset. <br> Workaround Downgrade to a version prior to 7.1.23 <br> Resolution Upgrade server to 7.2.1 or newer to address proper timeout detection and… Continue reading System watchdogs while archiving when SMB network share connection is lost