False Positive drives offline for disks labeled “sat” – invalid disk type errors Exacq Support has identified an issue with SMART attribute labels causing false positive drive offline errors on the hardware tab of ExacqVision Client. Some Disks may show error of “invalid disk type” Some systems may contain drives that get listed as… Continue reading False Positive drives offline status for disks labeled “sat” – invalid disk type errors
Tag: Smartctl
The Smartctl Copyright Notice May Be Unintentionally Inserted into the Server Logs
The Smartctl copyright notice may be unintentionally inserted into the server logs.
Storage Hardware Attribute Alarms from 3rd Party HDDs
Servers are reporting Health Warnings in exacqVision Enterprise Manager. The event details in EM show “This result is based on an Attribute check on Disk /dev/csmi0,2” Note: the device may vary for example /dev/csmi0,0 instead of csmi0,2 or perhaps both. The corresponding exacqVision Enterprise Manager logs show: It has been determined that these are false… Continue reading Storage Hardware Attribute Alarms from 3rd Party HDDs