Description Follow these instructions to silence MegaRAID alarms using LSI Storage Authority (LSA). Product Silence the Alarm When the controller detects an issue an alarm will occur and a high pitched beep will be emitted. This alarm can be silenced through the LSI Software Authority.
Tag: Silence
exacqVision – MegaRAID Silence Alarms
Title exacqVision – MegaRAID Silence Alarms Description This article describes multiple ways to silence MegaRAID alarms using either LSI Storage Authority (LSA) or MegaRAID Storage Manager (MSM). Also included is the storcli command, which can be run from a command or terminal line, regardless of which management software LSA or MSM is installed. Product exacqVision… Continue reading exacqVision – MegaRAID Silence Alarms
Resetting the Power Supply Alarm
Description Exacq built systems with redundant power supplies will emit an audible alarm in the event of a power failure. Here is how to silence the various models so you can enjoy peace and quiet while determining the cause of the failure. Product Solution The following photos show the location of the mute button on… Continue reading Resetting the Power Supply Alarm