Will not boot: USB device over current status detected will shut down in 15 seconds

Symptom:   System will not boot and you see the error:  USB device over current status detected will shut down in 15 seconds (the front logo light may also be out at this time) <br> Problem: The cable from the motherboard to the lit front cover is pinched. <br> Solution: Open the front cover and… Continue reading Will not boot: USB device over current status detected will shut down in 15 seconds

Creating a Shutdown Hot Key in Linux

To create a shutdown hot key on a Linux ExacqVision system, complete the following steps: Ubuntu 20.04 & 18.04 These systems are already configured to use CTRL+ALT+DEL to pop up a dialogue with a shutdown option. Once the dialogue opens the system will shutdown if no further user interaction occurs. Ubuntu 16.04 and earlier This… Continue reading Creating a Shutdown Hot Key in Linux